Science and sailing: A winning combination for our oceans
Sponsorship
10 octobre 2024
3 min
Ocean Calling conference

A groundbreaking study on marine pollution was presented on October 1st at Nexans’ innovation center, AmpaCity, in Lyon, born from a novel partnership between the scientific world and industry. United around Fabrice Amédéo, researchers unveiled unprecedented results obtained thanks to a cutting-edge sensor deployed during the 2020 Vendée Globe. This unique campaign revealed the omnipresence of microplastics in the ocean, their diversity, and the explosion in the number of small microplastics, as well as the presence of cellulose fibers. These major discoveries, made possible thanks to the collaboration with Nexans, could well change our perception of the health of our oceans.

Data that challenges scientific knowledge

The Imoca Nexans-Wewise, skippered by Fabrice Amédéo and equipped with a sensor measuring three fragment sizes (300, 100, and 30 microns), enabled scientists Enora Prado (Ifremer), Christophe Maes (IRD), and Sophie Lecomte (University of Bordeaux) to reveal, during the conference, the unprecedented dispersion of microplastics, independently of major ocean currents. This data, collected thanks to this advanced instrumentation, calls into question current knowledge about the dispersion of marine waste, as explained by Christophe Maes, an oceanographer at IRD. The Ocean Calling endowment fund, in collaboration with research teams, aims to model more precisely the impact of these microplastics on marine ecosystems.

AmpaCity: An innovation ecosystem serving the environment

Located in Lyon, the AmpaCity site, inaugurated in 2022, plays a central role in the Group’s mission. Spanning 6,000 m², with 4,500 m² dedicated to more than 20 laboratories, AmpaCity brings together a hundred experts from 10 different nationalities, including 17 PhDs, to develop cutting-edge technologies. The site focuses on key projects such as reducing environmental impact and increasing the reliability of electrical networks.

Microplastic pollution in the oceans concerns everyone, both individuals and industries. Acting on these issues is therefore essential, which is why the circular economy, with its challenges related to plastics, is one of the major topics addressed at the AmpaCity innovation center. For example, Nexans’ Mobiway range offers reusable packaging, an effort in line with the company’s commitment to the circular economy. In addition, Nexans is exploring the use of plastic waste to manufacture cables, a step aimed at reducing its carbon footprint.

The Vendée Globe, a platform for science

Fabrice Amédéo, who will once again take the start of the Vendée Globe in November 2024 with his boat equipped with the sensor, is proud to contribute to this citizen science initiative, hoping that the results will encourage a change in behavior and increased support for recycling and developing countries. It is essential to remember that 90% of marine waste comes from the major rivers of emerging countries, and that the fight against plastic pollution also requires strengthened international aid.

 

Watch the Ocean Calling conference replay below and learn more about these scientific revelations. Discover how these results contribute to the fight against ocean pollution and the advancement of solutions to reduce environmental impact.

First results provided in 2022 and 2023

First scientific results: results of measurements at 300 microns

This study, led by three French institutes: Ifremer, the University of Bordeaux and the IRD (a public research institution), reveals that the surface waters of the Atlantic Ocean are twice as polluted by cellulose fibres as it is by microplastics.

This study, based on measurements taken from an offshore race boat, also shows that the North Atlantic is more affected by plastic pollution than the South Atlantic and questions the dynamics of the subtropical gyre (area with a high concentration of microplastics) since the pollution levels measured there are lower than expected.

Results of the measurements at a precision level of 100 microns

All these measurement campaigns are analyzed by scientists from the University of Bordeaux and Ifremer.

The analyses indicate a significant presence of cellulose fibers in the filters: they are 40 times more concentrated on the 100 µm sieves with a distribution in the water column almost equivalent to that of microplastics. Another striking fact is that 100% of the samples from the 100 µm sieves contain microplastics compared to 64% for the 300 µm sieves.

By going from an analysis of 300 to 100 µm, the presence of microparticles (cellulose fibers and microplastics fragments) increases, and the proportion of microplastics is also on the rise: at 300 µm, there are twice as many cellulose fibers, at 100 µm, the proportion is 54% cellulose fibers and 46% microplastics.

Together, let’s protect our oceans.

Nexans, mécène de la restauration de la cathédrale Notre-Dame de Paris
Mécénat
02 février 2023
5 min
Notre-Dame de Paris Cathedral

Nexans annonce la signature d’une convention de mécénat avec l’établissement public chargé de la conservation et de la restauration de la cathédrale Notre-Dame de Paris, maître d’ouvrage, et contribue à la préservation du patrimoine français. Le Groupe met à disposition son expertise du câblage garantissant la sécurité incendie, et s’engage à faire don de près de 200 kilomètres de câbles de protection au feu Nexans Alsecure® afin d’équiper la cathédrale en cours de restauration.

Ces câbles serviront à distribuer l’énergie et équiperont Notre-Dame de Paris avec les techniques les plus évoluées sur le plan de la sécurité incendie. Les câbles de protection au feu Nexans Alsecure® produits et fournis par le groupe ont la capacité de significativement ralentir la propagation des incendies. Ils permettent également de réduire les émissions de gaz incapacitants et garantissent une faible émission de fumée pour faciliter les évacuations. Ce type de câble est également déjà déployé en France au sein d’établissements recevant du public, tels des crèches et des hôpitaux, et constitue l’engagement de Nexans pour anticiper les risques liés au feu, sécuriser les biens et protéger les personnes.

En tant que mécène, Nexans est fier de s’associer à la restauration de la cathédrale, symbole universel de Paris et de la France, et de contribuer ainsi à la conservation du patrimoine français. Nos collaborateurs sont mobilisés pour prendre part à cette aventure collective, incarnant ainsi l’une des valeurs fortes de Nexans : l’unité.

Christopher Guérin
Christopher Guérin

Directeur général, Nexans

Cet engagement est notamment rendu possible grâce à la forte mobilisation des salariés du Groupe des sites de Mehun-sur-Yèvre (Cher) et d’Autun (Saône-et-Loire), lieux de production de ces câbles qui seront mis à disposition à compter de l’été 2023.

Nous sommes très heureux de pouvoir bénéficier du mécénat en nature de Nexans qui nous apporte son expertise sur les câbles électriques ignifugés, nécessaires à la réouverture de la cathédrale en 2024. Nous sommes attentifs à doter la cathédrale des produits et équipements les plus performants, notamment en termes de sécurité incendie. Nous nous réjouissons que le savoir-faire français soit une fois de plus mis au service de la restauration de Notre-Dame de Paris. C’est une chance pour la France que des entreprises comme Nexans soient attachées à participer à la renaissance de notre patrimoine.

Jean-Louis Georgelin

Général d’Armée, Représentant spécial du Président de la République française, Président de l’établissement public chargé de la conservation et de la restauration, Cathedrale Notre-Dame de Paris

Suivez le chantier sur les réseaux sociaux

Dernières actualités

thumbnail-nexans-zaphiro

16 Juin 2025

Nexans et Zaphiro unissent leurs forces pour digitaliser le réseau électrique

Nexans et Zaphiro Technologies, entreprise suisse spécialisée dans la supervision et le monitoring avancés des réseaux électriques, annoncent un partenariat stratégique destiné à accompagner les opérateurs de réseaux publics et privés dans leur transformation digitale.

Navire de construction sous-marine tirant un tuyau orange dans l'eau bleue.

11 Juin 2025

Nexans électrifie la Crète : un câble sous-marin HVDC relie l’île au réseau électrique continental grec

Le 24 mai 2025, l’interconnexion Attique–Crète, le plus grand projet de transport d’électricité jamais réalisé en Grèce, est officiellement entrée en service.

02 Mai 2025

ChangeNOW 2025 : Nexans en action pour électrifier un avenir durable

Du 24 au 26 avril 2025, Nexans a participé à l’événement ChangeNOW, le plus grand rassemblement mondial dédié aux solutions pour la planète, en tant que partenaire officiel.