Electric seas

Subsea Interconnectors: The Giants Beneath the Waves

Picture a giant steel serpent. These aren’t mythical sea creatures—they’re subsea interconnectors!

These invisible arteries, comprising high-voltage cables laid beneath the sea, enable electricity to flow seamlessly between countries.

Diameter

Up to 300 mm

The girth of these marine giants

Weight

200 kg

Each meter can weigh up to 200 kg

Maximum Depth

3 000 m

Currently reaching
installation depths of 3,000 m (as of 2025)

Crafted with millimeter precision in state-of-the-art factories.

These subsea cables are transported aboard cable-laying vessels and deployed on the ocean floor.

A technological marvel enabling energy transmission across seas and oceans.

Projects Around the Globe

386

projects completed: Nexans has installed over 12,000 km of subsea cables and more than 400 km of terrestrial cables, representing a transmission capacity of 40 GW

Market Forecast

15%

of each European country’s electricity production is expected to be exported by 2030

Source: European Commission, Electricity Interconnection Targets

Miles of cables

+25 000 km

of high-voltage subsea cables will be installed in Europe between 2020 and 2030 matching the total installed over the previous 30 years!

Europe,
The Most
Connected Continent

Europe leads the way in interconnection technology, boasting an exceptionally sophisticated network that relies heavily on subsea cables.

Key Projects

Great Sea Interconnector (2028)

Crete to Cyprus

2×900 km HVDC cables,
the largest interconnection project in history

Facilitating energy exchange, integrating renewables, and powering 3 million homes.

Celtic Interconnector (2026)

France to Ireland

2×500 km HVDC cables, the longest in the world

Linking Ireland to mainland Europe for the first time, with a 700 MW capacity—enough to power 450,000 homes—while enhancing Ireland’s energy security.

Crete-Attica Interconnector

Crete to mainland Greece

335 km HVDC cable at 1,200 meters depth

Ensures Crete’s energy supply while transitioning from fossil fuels to wind and solar power.

NordLink Interconnector

Germany to Norway

2×700 km subsea cables with a 1,400 MW capacity

Enables the exchange and storage of renewable energy between Norway and Germany.

Europe, The Most Connected Continent

Europe leads the way in interconnection technology, boasting an exceptionally sophisticated network that relies heavily on subsea cables.

Key Projects

Great Sea Interconnector (2028)

Crete to Cyprus

2×900 km HVDC cables, the largest interconnection project in history,

Facilitating energy exchange, integrating renewables, and powering 3 million homes.

Key Projects

Celtic Interconnector (2026)

France to Ireland

2×500 km HVDC cables, the longest in the world

Linking Ireland to mainland Europe for the first time, with a 700 MW capacity—enough to power 450,000 homes—while enhancing Ireland’s energy security.

Key Projects

Crete-Attica Interconnector

Crete to mainland Greece

335 km HVDC cable at 1,200 meters depth

Ensures Crete’s energy supply while transitioning from fossil fuels to wind and solar power.

Key Projects

NordLink Interconnector

Germany to Norway

2×700 km subsea cables with a 1,400 MW capacity

Enables the exchange and storage of renewable energy between Norway and Germany.

Why Subsea Interconnections Matter

Securing and Balancing Grids

By linking power grids, energy can be redistributed where needed. Solar energy from Morocco can power Northern Europe, while Norway’s hydroelectricity can flow south.

This system enhances resilience by balancing surpluses and deficits.

Amplifying Renewable Energy Use

Excess renewable energy, instead of being wasted, can be transferred to regions with high demand.

Maximizing Socioeconomic Benefits

Enhanced interconnections translate to significant consumer savings through a more efficient energy network.

The Nexans Fleet:
At the Forefront

Cable-laying vessels (CLVs) are integral to the subsea interconnection process.

These technological marvels, some exceeding 100 meters in length, transport and deploy the cables with precision.

Subsea interconnections are transforming global power grids by enabling secure and efficient electricity exchanges between nations.

These colossal cables, installed at incredible depths, support renewable energy integration by directing surplus production to areas with high demand.

In Europe, the most connected continent, projects like the Celtic Interconnector and NordLink demonstrate the potential of these infrastructures to stabilize grids, reduce reliance on fossil fuels, and lower electricity costs for consumers.

With unmatched expertise and a modern fleet, Nexans is a key player in shaping a more collaborative, sustainable, and resilient energy future.

Find out more

Subsea interconnections for borderless electricity

Renewable energy

23 / 07 / 2024

Immerse yourself in the world of submarine cables and discover how innovative technologies are transforming the way we transmit renewable energy. Learn more about the sustainable solutions essential to powering our future efficiently and responsibly.

Explore