Context
In 2035, in Europe, combustion-powered vehicles will be banned, emphasizing the urgency of EVCI deployment.Β At the forefront of innovation, Nexans’ R&D center, AmpaCity, recognizes the pivotal role of Electric Vehicle Charging Infrastructure (EVCI) in advancing sustainable transportation. With a surge in electric vehicle (EV) adoption forecasted and stringent emissions regulations on the horizon, AmpaCity aims to lead by example. The installation of an EVCI at the Nexans R&D center not only facilitates employee access to EV charging but also serves as a model for future deployments.
Challenges
The implementation of EVCI at AmpaCity faced unique challenges, including the need for consensus among stakeholders, integration with existing infrastructure, and ensuring scalability for future expansion. Additionally, maintaining operational efficiency and minimizing disruptions during installation were critical considerations.
6
charging stations
30%
less time to install cables compared to classic installation
Nexans implication
Nexans leveraged its expertise in decentralized BUS & branch architecture to design and implement an efficient EVCI system at AmpaCity. Key aspects of Nexans’ involvement in the project include:
- Utilization of Nexans Cca – FR-N1X1G1-AR 0.6/1kV IRVE cables, Michaud connectors and Unex cable trays for robust and reliable charging infrastructure.
- Cables are Euroclass Cca ensuring visibility in case of fire allowing for safe evacuation (5 to 10 times less opaque smoke vs. R2V).
- Implementation of a BUS distribution system to optimize space utilization and accommodate future growth.
- Collaboration with internal and external partners to ensure seamless integration with existing infrastructure and operational continuity.
- Emphasis on time-saving installation methods, minimizing disruptions to daily operations at the R&D center.
By addressing challenges, providing innovative solutions, and actively participating in EVCI projects, Nexans plays a crucial role in accelerating the transition to sustainable transportation infrastructure.
The installation is quicker than an NF C15-100 star installation, and there are far fewer cable runs. It’s easy to fit into existing boreholes. All you have to do is install the new connections and protection to the new charging points. If there’s maintenance to be carried out, there’s no need to shut down the whole installation (…) no need to look everywhere for the main board key.
Installer Project Manager, Nexans