Superconductivity

Zero losses. 10ร— power density. Proven at scale.
High-Temperature Superconducting (HTS) cables and fault current limiters for power grids, hyperscale data centers, and offshore wind, with more than 20 years of field-proven deployments.

superconducting cable

10x

more current capacity
than conventional copper cables
of the same size

โ‰ˆ0

resistive energy losses,
zero heat generated in the conductor

3.2 GW

power in a single 17 cm cable,
equivalent to three nuclear reactors

-200ยฐC

operating temperature, reached with liquid nitrogen, inexpensive and harmless

20+

years of R&D and field deployments
across four continents

What is superconductivity?

Superconductivity is the complete loss of electrical resistance that occurs in certain materials when cooled to very low temperatures. First discovered in 1911, it has major implications for how electricity is transmitted, distributed, and protected.

High-Temperature Superconductors (HTS), discovered in the late 1980s, operate at -200ยฐC, a temperature easily reached using liquid nitrogen: an abundant, inexpensive, and environmentally harmless coolant. The superconducting conductor is immersed in a continuous nitrogen flow and enclosed in a cryogenic envelope that provides excellent thermal insulation.

Unlike conventional copper or aluminium cables, which lose 5-10% of transmitted power as heat over long distances, HTS cables conduct electricity with virtually zero resistance, meaning no heat, no energy loss, and no electromagnetic field emissions.

World leaders in flexible cryogenic envelope technology, with more than 20 years of proven expertise in HTS cable systems and superconducting fault current limiters (SFCLs).

Cryogenic systems
Five properties that change infrastructure design
These advantages hold across every application, from urban grid reinforcement to gigawatt data centers and offshore wind.

Zero energy loss

HTS cables have zero resistive losses, unlike conventional systems that dissipate 3โ€“10% of power as heat. The cooling energy is less than the transmission savings achieved.

Minimal footprint

Up to 10ร— less space than copper cables of equivalent capacity. Rights of way as narrow as 1 metre. No overhead lines, no wide trenches, no drying of surrounding soil.

Fault current limiting

Superconducting Fault Current Limiters (SFCLs) react within milliseconds to short circuits โ€” protecting transformers, switchgear, and downstream equipment automatically.

Zero heat & EMF

No heat emission regardless of transmitted power. No electromagnetic field interference with adjacent telecom, data, or pipeline infrastructure. Cables can be buried at greater depths.

No new tunnels needed

Existing pipes or tunnels can be retrofitted with HTS cables, considerably increasing transmission capacity without new civil engineering work.

Superconducting solutions by application

The same HTS platform, proven in urban grids for more than two decades, now addresses the power challenges of AI-era data centers, offshore wind, and future rail.

data centers

Hyperscale & gigawatt data centers

HTS cables carry up to 10x more power with zero heat, solving the space, thermal, and efficiency crisis in AI-era facilities. World-first LV AC & LV DC demonstration unveiled at Stella Nova, Hanover (2025).

Offshore wind farm

Subsea & offshore wind connections

A single 17 cm HTS cable delivers 3.2 GW at medium voltage, eliminating large conversion platforms and cutting offshore project costs by up to โ‚ฌ1 billion. SupraMarine project, funded by France 2030, demonstrator planned for 2028.

Chicago superconductivity project

Urban & transmission grid reinforcement

Market-proven HTS cables transmit 3-5x more power than XLPE cables at the same voltage, in corridors up to 10x narrower. Deployments in Essen (7+ years), Chicago, and Paris Montparnasse.

cryogenic systems

Cryogenic envelope & cooling systems

Every HTS system depends on world-class cryogenic engineering. Flexible vacuum-insulated piping (CRYOFLEXยฎ) maintains the โˆ’200ยฐC nitrogen flow, from cable joints to terminations.

Paris Montparnasse train station

Future rail & traction networks

Superconducting DC systems support high-speed rail traction by delivering higher currents over longer distances without energy loss, as demonstrated at Gare Montparnasse, Paris.

The industrialization of superconductivity is revolutionizing the path toward a more efficient and modern energy grid. With its advancing technology readiness and ongoing breakthroughs, superconductivity serves as a powerful catalyst for accelerating the energy transition and achieving Net-Zero targets.

Photo of Yann Duclot
Yann Duclot

Acceleration Units Director, Nexans

Success stories

Paris Montparnasse train station

Superconductivity

Strengthening the power supply at Montparnasse train station
Chicago superconductivity project

Superconductivity

Enhancing Chicago’s electric grid resilience

Frequently asked questions about superconducting cables

Talk to our superconductivity experts

Whether you are planning a grid reinforcement, a data center campus, or an offshore wind connection, our team can evaluate the business case for HTS technology on your project.

Innovation

4:50

Superconductivity: Powering a new era of energy infrastructure

Innovation

4:50

Superconductivity: Powering a new era of energy infrastructure

Interview

2:03

What is superconductivity? with Jacques Lewiner

Interview

1:33

What do you think about superconducting cables? with Charles Beigbeder